Friday, July 30, 2010
 

 
 
  Switch & Sensor Information   Switch & Sensor Terms
 
  What Is A Switch? Reed Magnets
  What is a Sensor? Hall Effect and MR Magnets
  What are the Different Types of
Switches and Sensors?
Mechanical Sensing Option M
  How is a Switch Used? Solid State Sensing Option E & Option I
  How is a Sensor Used? Source (PNP)
  How do I Choose
a Switch or Sensor?
Sink (NPN)
   
   
 
  What Is A Switch?
  A switch is a mechanical or solid state device that acknowledges when something takes place. Switches are mounted at the end of stroke on all PHD products to signal that the unit has reached full extend/retract, full clockwise/ counter-clockwise, or full open/close jaw movement. This is a combination of a switch and a magnetic field.
 
  What is a Sensor?
  PHD sensors are used only for rotary actuators and grippers. A sensor is an electronic Hall Effect device used to sense full open/close jaw movement on two separate grippers, or full clockwise/counter-clockwise rotation on two separate rotary actuators. A sensor can also be used to sense up to four positions on a single gripper or rotary actuator.
   
  What are the Different Types of Switches and Sensors?
  Hall Effect Switch, Hall Effect Sensor, Magnetoresistive Switch, Reed Switch, Inductive Proximity Switch.
   
  How is a Switch Used?
  PHD Compact Switches are available for most Tom Thumb® and PHD products. Their compact, low-profile design saves space and provides additional mounting flexibility. We also offer liquid resistant switches for use in applications where coolant or moisture is present.
   
  How is a Sensor Used?
  Switches are used to signify the end of stroke, rotation, or jaw movement. This is done using a magnet that is attached to a piston inside the tube. The switch will change states when effected by a magnetic field. When it comes into contact with the magnetic field, the switch is then enabled, or “turned on,” and a signal is sent to the load.
   
  How do I Choose a Switch or Sensor?
  There are many factors to consider when choosing the right switch or sensor. Most of these factors are listed on this page under 'Switch and Sensor Terms' below.
   
  Switch and Sensor Terms
   
  Reed Magnets
 
  • Option M must be ordered
  • Axial Polarity
  • 50 Gauss minimum
  Hall Effect and MR Magnets
 
  • Option E Hall Effect
  • Option I MR
  • Radial Polarity
  • 110 Gauss Minimum
   
  Mechanical Sensing Option M
  Mechanical sensing is PHD’s Reed Switch and applies to switches AC or DC. The switches are glass encapsulated for a long life and protection, with a typical life of 8 million cycles, and low cost.
   
  Solid State Sensing Option E & I
  Solid State Sensing is PHD’s Hall Effect or Magneto Resistive Switch. Applies to Switches DC only and has no moving parts. These switches have a typical life of forever.
   
  Source (PNP)
  PNP (Source) is what everyone is accustomed to, and is the most common switch.  It provides current to the load.
   
  Sink (NPN)
  NPN (Sink) is opposite of PNP (Source).  It provides a path to negative switching (true load).